Cell Specific Reference Signal (Advanced LTE FDD Downlink)

One cell specific reference signal is transmitted from each downlink antenna port.

The downlink cell specific reference signal can be used for the following purposes:

Additional Downlink parameters are described in Cell Parameters (Advanced LTE FDD Downlink), Positioning Reference Signals (PRS) - (Advanced LTE FDD Downlink), Synchronization Signals (Advanced LTE FDD Downlink), and Power Relevant Parameters (Advanced LTE FDD Downlink).

Cell specific Reference Signal Power

Range: -60 to 20 dB

Default: 0.000 dB

Enter a power level in dB for the cell specific reference signal.